Hi,
I want to analyze an up-converter. The IF mixer input is 33 channels (54 to 360 MHz). I want to up-convert with an LO of 1440 MHz.
In the System Simulation/Data, in the Path tab; what value of "Channel Frequency"do I put there for this simulation?
Thank you
I want to analyze an up-converter. The IF mixer input is 33 channels (54 to 360 MHz). I want to up-convert with an LO of 1440 MHz.
In the System Simulation/Data, in the Path tab; what value of "Channel Frequency"do I put there for this simulation?
Thank you
Questions regarding the use of the software should be in the Product Questions Forum. Support questions are tracked in that Forum and it creates a database that allows the support team to not only answer the question but to detect trends in questions to alert the documentation and software developers when something is unclear and needs to be improved.
Clear skies and high Q