See the attached file. I want to display the S21 of an amp and the large signal S21 of the amp on the same rectangular graph. Take a look at the "Bugged Gain chart" in the attached file. It appears that the LargeS(2,1) data and the S21 data have incompatible frequency data.
They display correctly on a polar chart.
Am I doing soething wrong? Is there a better way to do this?
Tony
[file]bfr106_2.wsp[/file]
They display correctly on a polar chart.
Am I doing soething wrong? Is there a better way to do this?
Tony
[file]bfr106_2.wsp[/file]
1) Near the top of the workspace tree, under the Analysis folder,
Fsweep1 (F/HB1) and Fsweep2 (F/HB2),
right-mouse click, on both of the above, Properties, and
change the Sweep Range
from Start Value: 135 to 135e+6
from Stop Value: 175 to 175e+6
and (because there are too many points)
change the Type Of Sweep
from Linear: Step Size: 5 to
from Linear: Number of Points: 9
2) Near the middle of the workspace tree, under the Design folder,
Port1 (Schematic) and Port2 (Schematic),
right-mouse click, on both of the above, Open, and
on the high-lighted schematic,
double left-mouse click on the input port to get the Port Properties,
change the Name, F, Source Frequencies: f
from MHz to Hz
Then update the simulation by a left-mouse click on the
Calculator button near the top-center of the workspace window.