I am using SpectraSys in Genesys 2007. Whenever I try to place a component in its non-default position, the components text gets flipped. A good example is the basic mixer component. When I place the basic mixer component on the schematic using a right-to-left motion, the entire mixer is upside down. Is there a fix to this problem, what am I doing wrong?
Yes, the flipped-text behavior is different from 2004 and earlier versions of Genesys. However, it is unlikely to change.
If you need to display the text "right side up", you will need to define a custom symbol and use it instead of the standard Mixer symbol.