How do you output, in either tabular or graphical form, a specific value or set of values from a matrix value. In a previous posting, Sergey suggested that individual matrix elements could be identified with the notation V[h,p], where h is the harmonic number and p is the port number. This was associated with the large signal S parameter functions in G2005. I have looked at the workspaces that were supplied on the Large signal S parameter posting, and none seem to give the correct answers-ie the large signal model data and the linear model data do not match at small signal conditions. I was then attempting to hard code the calculation (ie use the equations as shown in the Large signal library function), but was unable at this point to manipulate the data. I also would like to know what is the variable that describes available voltage at a port (to identify total incident power for the Large S parameter calculation.
https://edasupportweb.soco.agilent.com/pls/portal/support.show_topic?id=2107