How can one couple the tuned value of one component to another similar one, such as a tandem capacitor or resistor? . . or to tune a balanced bridge without breaking the balance? I am optimizing, not tuning manually, so orderly tuning multiple values at a time does not solve the problem.
I have tried to rename a part to match another existing part (R2 to R1, R1 existing), hoping that tuning one part will automatically modify the value of the renamed part. Genesys does not allow 2 parts with same number. I do not see a common tuning operator.
Is there a way to tune values in tandem?
I have tried to rename a part to match another existing part (R2 to R1, R1 existing), hoping that tuning one part will automatically modify the value of the renamed part. Genesys does not allow 2 parts with same number. I do not see a common tuning operator.
Is there a way to tune values in tandem?
e.g. in Equations widow, use
res_value=?1000
Then in the dialog box for R1 and R2 properties use "res_value". Now you can tune the value of R1 and R2 together.