Why do the graphs re-size upon program shutdown and boot up the next time around? For instance, I will size the windows for comfortable use. I will shut the program down, and the next time I boot the program up, the windows will come out tall and thin. Can this be set so that the windows will remain the same size as they were upon shutdown?
Window sizes are saved with the workspace so if you've rearranged them to suit you just save the workspace and they will come back at the same sizes. They do resize on load to fit the frame so enlarge the GENESYS window to the same size you had before saving and they'll come back identically.
Mark