Hallo,
I have some troubles with tune function in 2006.07. It has been improved and seems very powerful so, I investigate it in detail.
When I start a schematics and tune (ie: getting started example) the original state (R=50;C=1000pF) remains on the screen while I am tuning C1.C.
When I want to save, I have warnings because it can't save original. Is it normal ? I could understand it can't save but why to warn about it because there is no other choice ! Why not saving this "original" dataset
if needed ?
I can create "better" and "best" curves as in the manual. I suppose I need to use the floppy icon to save these states because otherwise, they don't appear anymore in the list box.
When I want to save, I have warnings because it can't save original, better and best. Is it normal ? Again, why can't we save these 3 datasets ?
Of course, when I reload the file, the three states have disappeard even if I used the floppy icon.
If I try to tune another time, the response changes but the "original" is not displayed anymore on the screen while tuning. Is there an option to leave the curve displayed or, in another words, why the original diplayed only at first run of the schematics ? I have seen that .original appears in the graph properties but why only once ?
Best regards
Marc
I have some troubles with tune function in 2006.07. It has been improved and seems very powerful so, I investigate it in detail.
When I start a schematics and tune (ie: getting started example) the original state (R=50;C=1000pF) remains on the screen while I am tuning C1.C.
When I want to save, I have warnings because it can't save original. Is it normal ? I could understand it can't save but why to warn about it because there is no other choice ! Why not saving this "original" dataset
if needed ?
I can create "better" and "best" curves as in the manual. I suppose I need to use the floppy icon to save these states because otherwise, they don't appear anymore in the list box.
When I want to save, I have warnings because it can't save original, better and best. Is it normal ? Again, why can't we save these 3 datasets ?
Of course, when I reload the file, the three states have disappeard even if I used the floppy icon.
If I try to tune another time, the response changes but the "original" is not displayed anymore on the screen while tuning. Is there an option to leave the curve displayed or, in another words, why the original diplayed only at first run of the schematics ? I have seen that .original appears in the graph properties but why only once ?
Best regards
Marc
The warnings are because it deletes the graph checkpoints when you save a file and the graph isn't updated appropriately. It's a pretty minor issue that's fixed in the next version.
Graph checkpoints do not persist; they are only intended for display while the program is running. If you want saved checkpoints you should checkpoint the tuned values by using the disc icon. These are saved when you save the file.
Mark