AnsweredAssumed Answered

Frequency Plot HB VCO Sweep

Question asked by rfehn on Aug 16, 2010
Latest reply on Aug 16, 2010 by SERGEYTRU
Hi
For a VCO HB sweep I can plot the output power of the oscillator as a function of varactor voltage by making an equation like  P1[Freq@Freq[2]] or                     hb_getspcompdbm(P1, FreqIndexIM,1 ). I would also like to plot the fundamental frequency of the VCO as a function of varactor voltage in the same graph, but I can't find out how (I only manage to plot the frequency as a function of inex). Can anyone help?

Roy  

Outcomes