Can someone point me to literature that derives the differential gain and match of a four port mixed mode network based on standard four port S parameters where, in the final circuit the common mode excitation at ports 1 and 3 is zero, the load at ports 2 and 4 are well matched, and the network has full symmetry?
Thanks, Trevor.
P.S. A typical example might be a balanced amplifier using 180 degree full hybrids.
Thanks, Trevor.
P.S. A typical example might be a balanced amplifier using 180 degree full hybrids.
http://downloadfile.anritsu.com/RefFile ... 00279B.pdf
I hope this is useful to others!
Trevor.