AnsweredAssumed Answered

2002.09 versus 2003.10 ???

Question asked by vorlan on Oct 27, 2006
Latest reply on Oct 30, 2006 by vorlan
Can any one tell me why in the in the 2002.9 version when it is in optimizing routine I can stop the optimization (ESC) and I can choose to go back to the dotted trace or update to opt. trace (F5) and when I do the same in the 2003.10 if there is any equation block , will go to the last optimized run ,but it will work just fine if not equation block variable it is present in equations windows

[version numbers have been edited to reduce confusion]  

Outcomes