AnsweredAssumed Answered

Why to not add link between vendor part list and layout

Question asked by enrico_lia on Nov 6, 2006
It would be nice if we could have Genesys Eagleware operating with vendor symbolsbetween schematic and layout, in e.g. BJT transistor BFP620 from Infineon with 4 terminals, so we could see the it in both windows.

I am not talking about to increase library, but create a SOT-343 footprint for many common terminal designation existed with all other vendors.

It is being difficult to create and later on associate a new schematic symbol with layout and use it with nonlinear model. Normally the two first are not complicated, but when loading the nonlinear model...it becomes to be a problem.

Thanks.  

Outcomes