AnsweredAssumed Answered

Equations Example (RMS Calculation)

Question asked by pkarasev on Sep 6, 2006
The attached example shows a basic use of the equations in Genesys. A signal x(t) is constructed from scratch in equations and some calculations are performed.

The following are illustrated:

1) Creating and allocating vectors

2) Setting an independent vector (time) for a dependent vector x(t)

3) Performing calculation on vectors

4) Setting units for vectors

5) Plotting vector variables with correct axes and units

[file]rms_calculation_equations.wsx[/file]

Outcomes