I'm using Spectrasys to do some transmit line up calculations. I've built a simulation of the transmit lineup, and I'm looking at the spectral plot at the output. There are quite a few traces there, that I assume are contributions from each of the blocks in the simulation. How can I
1-Tell which block is contribuiting which trace
2-Get a single trace that shows the overall output spectrum?
This is in Genesys 2008.07 SP1
Thanks
Dave
1-Tell which block is contribuiting which trace
2-Get a single trace that shows the overall output spectrum?
This is in Genesys 2008.07 SP1
Thanks
Dave
Still not sure of #2, though.