AnsweredAssumed Answered

2009.04 input missing on basic toolbar

Question asked by RADIOONE on Aug 21, 2009
Latest reply on Aug 24, 2009 by RADIOONE
I am using XP professional as the operating system (not using classic view) running Genesys 2009.04 and I find that the input icon on the toolbar doesnt do anything, and the output icon is the one that produces the input drop down menu. The ground icon behaves as the output one and so on. I find Genesys 2008.07 is ok.  

Outcomes