Hi,
Now I want to use TEM TLRLGC to model transmission line S-para measured data.
I have a question on this parameter definition.
According to this manual, each parameter should be in per unit length though, is this unit meter or inch?
Thanks in advance,
Umekawa
Now I want to use TEM TLRLGC to model transmission line S-para measured data.
I have a question on this parameter definition.
According to this manual, each parameter should be in per unit length though, is this unit meter or inch?
Thanks in advance,
Umekawa
The per-unit parameters are used in the model equations in products with LEN: R*LEN, G* LEN, etc.
Before Genesys 2005.11 the parameters related to LEN units, because Genesys did not use units conversion.
Starting from Genesys 2005.11 Genesys internally always uses MKS units, and all the parameters must be "per meter".
Sergey