AnsweredAssumed Answered

Stripline Definition

Question asked by MUGU57 on Oct 10, 2004
Latest reply on Oct 18, 2004 by JERRY_MARKETOS
One question just to be sure that I understand the handbook correct.
If I want to make use of stripline (Triplate) instead of microstrip.
1. I am uning the relevant modells thats clear
2. I define the same substrate like for a microstrip
3. but then I change the optional substrate height parameter in each circuit / model,
which is normally empty as it normally take the substrate height from the substrate definition,
to twice the substrate height if i have a symmetracil stripline cross section

Is this correct?
Kind regards Michael  

Outcomes