Hi,
I have a very simple Eagleware workspace with just a data file (S2P) that I am trying to plot (it is attached). I can plot the S parameters and the real data (RE[S11]) but the imaginary data shows only zero when plotted. I do not think that this is what the data file contains since when I look at the circuit on my NWA it has some features. Can someone explain what is going wrong here?
Thanks,
Sean
I have a very simple Eagleware workspace with just a data file (S2P) that I am trying to plot (it is attached). I can plot the S parameters and the real data (RE[S11]) but the imaginary data shows only zero when plotted. I do not think that this is what the data file contains since when I look at the circuit on my NWA it has some features. Can someone explain what is going wrong here?
Thanks,
Sean
[file]problem_displaying_im[s11].wsp[/file]