Hello All,
I am new to ADS and I have following questions.
1. I tried to probe voltages at different nodes by labeling them with "Wire/Pin Label". But, I am not able to see them in the dataset. Do I need to enable some option to dump these voltages ? I can see currents with currentprobe
2. I am using "ClockWJitter" to generate clock. It drives a NMOS. When I plot NMOS current Vs. Time, it shows steady value and not changing with time. I have envelope simulator in the design. What should I do ?
Thanks,
Viral
I am new to ADS and I have following questions.
1. I tried to probe voltages at different nodes by labeling them with "Wire/Pin Label". But, I am not able to see them in the dataset. Do I need to enable some option to dump these voltages ? I can see currents with currentprobe
2. I am using "ClockWJitter" to generate clock. It drives a NMOS. When I plot NMOS current Vs. Time, it shows steady value and not changing with time. I have envelope simulator in the design. What should I do ?
Thanks,
Viral
Your post came to the RFDE forum, I am not sure it what you are seeing or not seeing is in RFDE?
Issue 1: Â You should be able to see all name nodes when you do a DC simulation, in addition you should be able to DC Back Operating points to the schematic. Â
Issue 2: Â The ClockWjitter (Voltage Source: Clock with Jitter) is a time domain source, it is the right source to generate clock.
I suggest emailing your two questions to our support organization: Â eesof_support@agilent.com, stating if this is in ADS or RFDE. Â Also, for the second issue, if you could be more specific in the issue, better yet, if you have an example of what you are seeing will be best.
I hope this is of help to you,
Thank you.