AnsweredAssumed Answered

Dataset overide

Question asked by CKOH on Aug 9, 2007
Latest reply on Aug 10, 2007 by JERRY_MARKETOS
When using a dataset file for a component, all of the parameter files are overidden.  It's often useful to be able to select which ones to overide. For example when using the Amp (2nd and 3rd order) component,if i have a s-parameter dataset without noise parameters, it would be convenient to set the noise figure.  Manafuctarers very often supply s-parameters without noise parameters.  

Outcomes