AnsweredAssumed Answered

.

Question asked by VRFuser on Jun 5, 2000
Latest reply on Feb 11, 2004 by VRFuser

----- Original Message -----
From: Shawn Wheelock <shawnw@cats.ucsc.edu>
To: <vrf@hplvlrx.lvld.hp.com>
Sent: Saturday, May 27, 2000 1:31 AM


> I am having two problems...
>
> 1) I need to be able to programatically and on the fly determine what type
> a piece of data returned from a record is within an if statement (if it is
> a number, I need to round it off, if it is a string, I need to do
> nothing).  I know C and Java have nice little functions which tell you
> that. I could find no such thing here.
>
> 2) I need to display on a plot (X vs. Y) AND ( X vs Z or Y vs Z ) -- on
> the same set of axes.  Can VEE do this?  I have not been able to find a
> way.
>
> 1)here is another solution,
you can use the "round" function and an error output to bypass a
string,see attached file.

       Regards Joergen





Outcomes