AnsweredAssumed Answered

AW: vrf showpannel

Question asked by VRFuser on May 24, 2000
Hi Justin.
If you only want to have a panel of a user function to have the same size
than the main panel the easiest way ist to read the main panels size with
PanelSize("Main").
See my little example and note that the sizes only fit correctly in runtime.
Hope it helps
     Georg Nied
Software-Development
Test and Measurement
51149 Cologne Germany
  gn-software@gmx.de

> -----Ursprungliche Nachricht-----
> Von: owner-vrf@hplvlrx.lvld.hp.com
> [mailto:owner-vrf@hplvlrx.lvld.hp.com]Im Auftrag von Justin Pallas
> Gesendet: Montag, 22. Mai 2000 13:29
> An: vrf@lvld.hp.com
> Betreff: vrf showpannel
>
>
> Hey guys,
>
> Have an easy questions.  When you do a showpanel command,
>
> i have the formula as ShowPanel("panelname", "cordinates")
>
> now i am going to be running this on various screen sizes, and
> was wondering if there is a comand string for the cordinates that
> will automaticly maximize it to the size of the window being used.....
>
> Any help on this is always greatly appreciated,
> Thanks guys
> Justin Pallas
> TRMI Inc, QA-Lab, PV Tech
>
> ---------------------------------------------------------------------
> This is the "vrf" maillist, managed by Majordomo.  To send messages to
> this maillist, just email to "vrf@lvld.hp.com".  Subscriptions and
> unsubscriptions are done through the address "vrf-request@lvld.hp.com".
> If you need details, just send a message containing the text "help"
> to "vrf-request@lvld.hp.com".
> ---------------------------------------------------------------------

---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.hp.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.hp.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.hp.com".
---------------------------------------------------------------------

Outcomes