AnsweredAssumed Answered

vrf 1 panel on top of the other - solution

Question asked by VRFuser on Jul 11, 2000
Dear all,

My problem was that I had two user function panels one being called after the other and then the panel of the second is residing on top of the background of the first panel but was disappearing as soon as I clicked somewhere else on the background.

The general comment to have the lock panel position in the general tap of each user function did the trick and it now works nicely.

Thanks lots for your help and time

Peter





Dr. Peter Braun
Royal Veterinary and Agricultural University
Dept. of Agric. Sci.
Sct. Horticulture
Agrovej 10
DK-2630 Taastrup
Denmark

Tel: +45-35 28 35 34
Fax: +45-35 28 34 78
Email: PBR@KVL.DK

---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------

Outcomes