AnsweredAssumed Answered

vrf File Requester/Excel

Question asked by VRFuser on Jul 12, 2000


I am using the VEE "File Name Requester" and activeX to save an Excel file
(Excel is running in the background). This works fine if the filename does not
already exist. But if it does, the "this file exists, overwrite?" requester
appears first on the VEE window, and after clicking "yes", it appears again on
the Excel window where it is hidden under the VEE window; this gives the
appearance of the machine being frozen. Is there a pretty way to force Excel to
overwrite an existing file under ActiveX without bringing up a hidden requester?

---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------

Outcomes