AnsweredAssumed Answered

Controlling export of data from EMPro

Question asked by thpreuss on Nov 22, 2011
Latest reply on Nov 28, 2011 by MARCP
We are exporting the data now and able to decode it for further processing. There is a problem however, on the Export field data dialog box there is an entry field labeled 'Divisions', I assumed that this could be used to set the number of divisions that the data is sliced into (for example the default value 20 means 20 by 20 by 20) however when I change this to anything other than 20 the same output is generated ie the default 20 divisions, am I doing something wrong or is this suppose to be like this. Ideally I would like to control the number of slices in all directions. Thanks for your help  

Outcomes