Presently ( or as far as I can tell) the gain circles are not marked. The center of the first circle is represenative of the maximum gain and the perrihery of each circle is a -1dB from the maximum. Is it possible to have eagleware calculate the max gain and have the marker display the gain of each circle.
Mark Zachmann
VP of R&D
Eagleware