AnsweredAssumed Answered

Notes page is doublespaced

Question asked by JERRY_MARKETOS on Jun 24, 2004
I think this started in version 2003.10, maybe earlier.
When typing in the NOTES page, you may notice double line
spacing occurs when you hit a carriage return.
You may also notice in newer versions of software, the notes
page is now gaining more ability to manipulate the text - colors,
text features, etc.  This is part of an enhanced feature set for the
text handling, and something that "automatically" comes with that
is...  automatic paragraph formatting of the text, which is what's
initiating the "automatic" double line spacing.

To avoid the double line spacing, just do a SHIFT + ENTER
and you'll get single line <CR>  

Outcomes