The latest Eagleware license server (20007.03 SP1), will install OK, and run, until you have to restart the server. Upon reboot, the server returns this error message:
Data Execution Prevention – Microsoft Windows
To help protect your computer, Windows has closed this program.
Name: Eagle.exe
The error occurs only if you have a chip that allows for Windows to run a more secure memory control called DEP (Data Execution Prevention).
Microsoft's solution for Windows Server 2003 PCs is listed below, the links below will take you to the original Microsoft support document for Server 2003 PCs and for Windows XP and Tablet PCs:
Windows 2003 servers:
http://support.microsoft.com/kb/875352
Windows XP and Tablets:
http://support.microsoft.com/kb/875351
.....If you are logged on as an administrator, you can manually configure DEP to switch between the OptIn and OptOut policies by using the Data Execution Prevention tab in System Properties. The following procedure describes how to manually configure DEP on the computer:
[list=1:ma1zl2hp]
Click Start, click Run, type sysdm.cpl, and then click OK
Click the Advanced tab, click Performance, and then click Settings
On the Data Execution Prevention tab, use one of the following procedures:
To configure DEP to switch to the AlwaysOn policy by using the Boot.ini file, follow these steps:
[list=2:ma1zl2hp]
Click Start, right-click My Computer, and then click Properties
Click the Advanced tab, and then click Settings under the Startup and Recovery field
In the System startup field, click Edit. The Boot.ini file opens in Notepad
In Notepad, click Find on the Edit menu
In the Find what box, type /noexecute, and then click Find Next
In the Find dialog box, click Cancel
Replace policy_level with AlwaysOn. WARNING Make sure that you enter the text accurately. The Boot.ini file switch should now read: /noexecute=AlwaysOn
In Notepad, click Save on the File menu
Click OK two times
Restart the computer
Data Execution Prevention – Microsoft Windows
To help protect your computer, Windows has closed this program.
Name: Eagle.exe
The error occurs only if you have a chip that allows for Windows to run a more secure memory control called DEP (Data Execution Prevention).
Microsoft's solution for Windows Server 2003 PCs is listed below, the links below will take you to the original Microsoft support document for Server 2003 PCs and for Windows XP and Tablet PCs:
Windows 2003 servers:
http://support.microsoft.com/kb/875352
Windows XP and Tablets:
http://support.microsoft.com/kb/875351
.....If you are logged on as an administrator, you can manually configure DEP to switch between the OptIn and OptOut policies by using the Data Execution Prevention tab in System Properties. The following procedure describes how to manually configure DEP on the computer:
[list=1:ma1zl2hp]
- Click Turn on DEP for essential Windows programs and services only to select the OptIn policy
- Click Turn on DEP for all programs and services except those I select to select the OptOut policy, and then click Add to add the programs that you do not want to use the DEP feature.
- Click OK two times
To configure DEP to switch to the AlwaysOn policy by using the Boot.ini file, follow these steps:
[list=2:ma1zl2hp]