Hello,
Why example: Amplifier SiGe BFP620 works correctly under Harbec with V2002.09, but gives erroneous resultats with the new V2003.03 version.
To make test, to compare resultats with 2 versions.
OS is W2000.
Thanks
Why example: Amplifier SiGe BFP620 works correctly under Harbec with V2002.09, but gives erroneous resultats with the new V2003.03 version.
To make test, to compare resultats with 2 versions.
OS is W2000.
Thanks
If you change Harbec to use Automatic Jacobian (rather than Always) I think you get the correct results.
I believe that this is actually a bug-fix in 2003.03 such that Jacobian Always now correctly always uses the Jacobian - but that does not converge for the SigE example.
We do have a fix for just the executable available (tentatively called SP3) that you can download if you wish. The only change to this version (compared with SP2) is bug-fixes in Harbec HB Analysis.
Please contact us directly for directions on how to do that so that we can verify your license.
Mark Zachmann