I recently created a user model from a schematic. It had three numbered ports. It also had several ground connections in the middle of the schematic.
When I tried to instance the model in another workspace, I used a three-port with ground. That resulted in an error message stating that I had the wrong number of ports. After much fiddling around, I discovered that if I used a three-port without ground, the error messages would go away.
What do I have to do to a user model to get it to use a ground connection when it is instanced? Add a port with the final number to the ground node?
When I tried to instance the model in another workspace, I used a three-port with ground. That resulted in an error message stating that I had the wrong number of ports. After much fiddling around, I discovered that if I used a three-port without ground, the error messages would go away.
What do I have to do to a user model to get it to use a ground connection when it is instanced? Add a port with the final number to the ground node?
Rob Lefebvre