AnsweredAssumed Answered

EM Power Viewer Problem

Question asked by jrambe on Nov 12, 2003
Latest reply on Nov 24, 2003 by jrambe
Hi

I' m evaluating Genesys Version 2003.03 and am currently looking at EM Power. I' ve opened the LNMIT3 example without problems, but when choosing Run EMPOWER Viewer in the Workspace window I get an error message: "Error locating necessary initialization files". It is suggested that the files EAGLEWIN.INI or DEFAULT.EG$ are either invalid or do not exist. They do exist in the correct directories, and I' ve tried to un-install and re-install Genesys to correct the problem, without the problem being solved. For your information the Genesys software is installed locally on my laptop.

Hope you can help

Best regards, Jan  

Outcomes