My company has just upgraded to 2003 on the NT networked workstations and I am not able to use the synthesis tool for A/FILTER - it locks up!. Under 8.01 the synthesis pull-down menu contained all of the licensed tools - now only PLL and TLINE show. The remaining filter synthesis tools can be right-click accessed via the folder now showing up in the workspace folders window. When I select add A/FILTER the program loads it into the workspace. When I start changing parameters to synthesis a filter the whole application locks up and I may get a fatal error message. I then have to END TASK under the manager.
I have done this multiple times and have achieved multiple lock-ups.
I need help and explaination to why the synthesis tools no longer run and no longer are under the pull-down menu. Any suggestions?
I have done this multiple times and have achieved multiple lock-ups.
I need help and explaination to why the synthesis tools no longer run and no longer are under the pull-down menu. Any suggestions?
The synthesis programs are no longer on the menu because they are now built-in and are created in the same way everything else in GENESYS is created: through the workspace manager/tree.
Rob Lefebvre