RFDE crashes when netlisting design. When RFDE is first loaded and design is opened, netlister works fine on circuit. If I change the slightest parameter, regardless of the parameter, the netlister crashes RFDE without an error in the CDS.log. This is the last line in the log file:
\o Begin Incremental Netlisting Dec 16 17:46:11 2003
Then all windows disappear.
RFDE 2003C R202
Linux Redhat 8.0
\o Begin Incremental Netlisting Dec 16 17:46:11 2003
Then all windows disappear.
RFDE 2003C R202
Linux Redhat 8.0
please refer your questions in this issue to eesof_support@agilent.com
Thank You.