AnsweredAssumed Answered

programmatically addressing RS232 interface event & bus IO monitor

Question asked by VRFuser on May 16, 1999
Latest reply on May 16, 1999 by VRFuser


NANCY_MOREYRA@HP-Seattle-om1.om.hp.com wrote:

> Does anyone know of a way to programmatically set the address of
> the bus IO Monitor or DAV in the RS232 interface event?

Hello Nancy,

I think this is no way to program DAV object to change the logical number
of the port at run time, because it haven't control input pin to address
it.

HP migth think about because DAV object allows implement interrupt
algorithms instead of polling algorithms.



Outcomes