AnsweredAssumed Answered

motor controlling

Question asked by VRFuser on Jun 2, 1999
Hello Scott,

over a plug-in card the field bus " AS INTERFACE " can be coupled with a PC and HP VEE. The company " Siemens " developed a Slave in co-operation with the company "Bihl und Wiedemann" for
the control of a frequency static frequency changer. We did not test these however yet. Theoretically the possibility exists to thus regulate over a two-wire line up to 31 engines into 300
meters distance.

Yours sincerely of Nils Remer
* * * * * * * * * * * * * *
  Dipl.-Ing. Nils Remer
  Geschftsfhrer

  AUTTEC NILS REMER
  Hagenower Strae 73
  D-19061 Schwerin

  Fon   +49 385 3993-440
  Fax   +49 385 3993-446
  email auttec@ani.de
* * * * * * * * * * * * * *



Outcomes