Hi,
I'm trying to simulate in the ICCAP 2004 PC version with windows XP. I set ADS_DIR variable in the Control panel/System/Advanced/Environment Variable as my local installation directory of ADS 2004A. But there is an error message that
UNABLE TO LAUNCH SIMULATOR
PROCESS TERMINATED UNEXPECTEDLY
SIMULATOR FAILED-DATA UNCHANGED
SIMULAOTR:hpeesofsim
PAth: C:\SoftWare\ICCAP_2004\\bin\hpeesofsim_start.exe
Use Simulation Debugger for more inofrmation
while I simulate in the model window.???
How can I solve this problem?
Thanks,
Sung-jin
I'm trying to simulate in the ICCAP 2004 PC version with windows XP. I set ADS_DIR variable in the Control panel/System/Advanced/Environment Variable as my local installation directory of ADS 2004A. But there is an error message that
UNABLE TO LAUNCH SIMULATOR
PROCESS TERMINATED UNEXPECTEDLY
SIMULATOR FAILED-DATA UNCHANGED
SIMULAOTR:hpeesofsim
PAth: C:\SoftWare\ICCAP_2004\\bin\hpeesofsim_start.exe
Use Simulation Debugger for more inofrmation
while I simulate in the model window.???
How can I solve this problem?
Thanks,
Sung-jin
For the link to ADS2004A on PC, one must define
one additional Environment Variable:
After you have defined ADS_DIR, to be, for example:
C:\ADS2004A
Then please define ICCAP_OPEN_DIR to be:
%ADS_DIR%\adsptolemy\lib.win32
Please then restart IC-CAP 2004.
This should resolve the issue you are seeing.
If you still see an issue or problem after defining
this variable, please call your local Agilent EESof
Technical Support:
http://eesof.tm.agilent.com/support/
Best Regards
Else