AnsweredAssumed Answered

VRF - 8752 Network Analyzer Calibration

Question asked by VRFuser on Apr 8, 1999
Latest reply on Apr 8, 1999 by VRFuser

Kevin,

What you will need to do is an execute for the DDE transaction with
the following for the command "[SAVE.AS("filename.xls")]" . The
backslashes in the command embed double quotes (") around the filename.
Filename could be replaced with an input variable by using the following
syntax "[SAVE.AS("" + A + "")]"

Hope this helps,

Lyle Carnahan
Hewlett-Packard
lyle_carnahan@hp.com


-----Original Message-----
From: Non-HP-MishKS /HP-USA,mimegw5/dd.HPMEXT1=MishKS@NSWC.NAVY.MIL
Sent: Friday, April 09, 1999 12:47 PM
To: hpvxd-xc-at-lvld
/HP-USA,mimegw5/dd.HPMEXT1=hpvxd_xc@hpislsup.lvld.hp.com
Cc: Non-HP-MishKS /HP-USA,mimegw5/dd.HPMEXT1=MishKS@NSWC.NAVY.MIL
Subject: VRF-need_help_with_DDE


Hello.

I'm writing a HP VEE program that will open an Excel spreadsheet,
dump data into it, then request a filename and save the spreadsheet
as that filename.

The only part I cannot determine is the command used for "SaveAs"
in Excel through the DDE.

Can anyone help?

Thanks in advance,
Kevin Mish
mishks@nswc.navy.mil

Outcomes