Hi,
I am trying to connect to a HP 3562A Dynamic Signal Analyzer (DSA) using MATLAB, with a NI GPIB-USB-HS cable. I have a VISA connection established with the DSA and am trying to send out simple commands such as "FRS?", but any command sent it (no matter the complexity), will get timed-out. The programming manual is written in BASIC, do not know if I am missing something in the syntax or it is more fundamental than that. Would be extremely grateful for any guidance on what I could potentially do. Is there a compatible syntax or a work around?
Thanks a million.
I am trying to connect to a HP 3562A Dynamic Signal Analyzer (DSA) using MATLAB, with a NI GPIB-USB-HS cable. I have a VISA connection established with the DSA and am trying to send out simple commands such as "FRS?", but any command sent it (no matter the complexity), will get timed-out. The programming manual is written in BASIC, do not know if I am missing something in the syntax or it is more fundamental than that. Would be extremely grateful for any guidance on what I could potentially do. Is there a compatible syntax or a work around?
Thanks a million.
Regards
Edited by: instrumentdriver on Apr 1, 2016 2:59 AM