AnsweredAssumed Answered

Problems in designing oscillator

Question asked by sara on Oct 27, 2011
Latest reply on Oct 27, 2011 by sara
Hello,
I should design an oscillator just consists of inductors and capacitors . the circuit should not have any resistors.
also, It has 4 MOSFETs instead of Not Gate. the lenghth of each inductor should be low, but the number of them are high. (as the schemes have shown below)
I designed and tested in every situation that I thought. The problem is that there is not resonable scheme after the simulation.
Any help will be appreciated.
Please see attached.
Image
Image

Attachments

Outcomes