AnsweredAssumed Answered

Harmonic Balance Power Spectrum (newbie question)

Question asked by raudabaugh on Apr 7, 2011
Latest reply on Apr 28, 2011 by R13801
Image
Image

Hi, I am trying to use the power spectrum to look at this P_1Tone and want to make sure I have set it up correctly.  The input is 2.45 GHz 0 dBm (or 0.001 W), but when I simulate, I get a value of 0.0002 at 2.45GHz.  Now, is this measurement in dBm, W, or something else?  If it's in W, why is it so far from 0.001?  

Outcomes