AnsweredAssumed Answered

Will IO Libraries 16.3 get data from a generic "virtual com port"?

Question asked by greif on Apr 5, 2016
Latest reply on Jun 10, 2016 by hognala
I have a new project where I need to grab a voltage from a  34410A  DMM (via USB?, other possibilities better?) and a number string from a USB micro-controller which appears  as a "virtual com port via USB".  (running win XP or Win 7)

These will form a data pair, and be gathered at about 600/sec.( about 30,000 pairs are to be captured)

Question: Can I use IO Libraries 16.3 to get data from the "virtual com port via USB"?

If not what can I use to grab both these data?

Thanks!

Edited by: greif on Apr 5, 2016 2:40 PM  

Outcomes