AnsweredAssumed Answered

34901A Usage

Question asked by badgerpaintball on Mar 21, 2016
Latest reply on Mar 23, 2016 by tomc
I would like to use the 34901A as a MUX for bank 1, and measure a thermocouple on bank 2.  IS this possible?

I would like to route channels 1-3 through the COM (Source) to power my unit.  I would switch between the different inputs to target different points on the UUT.

I will need one of the channels (1-3) to remain on while I am measuring the temperature using a thermocouple on say channel 11 or greater.

Can I separate the banks like that, or do I have to do the temperature measurement, and then re-configure the card to be the mux?  

Outcomes