I'm wondering if there are any compatability issues with ADS on Windows Vista.
I've seen that many software programs are having problems with Vista and I've also heard the same thing from the national news.
What version(s), if any, of ADS today are officially supported on Windows Vista?
If none are officially supported, will there be an ADS2006B released that will be supported and what will be the time frame for this release?
Thanks,
Mike
I've seen that many software programs are having problems with Vista and I've also heard the same thing from the national news.
What version(s), if any, of ADS today are officially supported on Windows Vista?
If none are officially supported, will there be an ADS2006B released that will be supported and what will be the time frame for this release?
Thanks,
Mike
ADS version 2006A and earlier are not compiled or tested in Windows Vista, and therefore we do not support these ADS versions running on Vista editions of Windows OS. They *may* install and appear to run properly. We just cannot guarantee the proper operation of ADS running on Vista platforms.
From what I understand - and it's been this way for years - no additional OS support is added with off-cycle releases such as a "B" verison of ADS. Typically only full-numbered releases (2006, 2005, etc.) either add new OS support or drop support of older/obsolete OS versions.
I will check with our internal R&D and Product Planning to see if we have any plans to support Windows Vista editions in ADS 2008 (our next ADS release) or beyond. I'll post here what I find out.
Regards,
Jay Mc Kee
Agilent EEsof Tech Support