I will like to simulate the phase noise of a BJT amplifier including flicker noise sources for the Ic and Ib currents, the parameters of theses sources like Kf and Af i have extracted through measurements. I have seen that ADS has a noise current source I_NoiseDB that can produce flicker noise components.When I try to implement the source of the schematic I dont understand what should I put for the "Element" and "Pin" values and how I can associate them with the base and collector currents of my device. Any help will be apreciated