AnsweredAssumed Answered

Simulate S-param file with more than 99 ports?

Question asked by mkobasa on Jan 3, 2007
Latest reply on Jan 5, 2007 by mkobasa
I'm wondering how I can simulate an S-parameter file with more than 99 ports in ADS.  

Say for instance I have a .s110p file with 110 ports, the component S110P does not exist in ADS.  I've seen example AEL code to generate an SS110P component in the networks directory and I tried that and was able to create the component.

However, when I try to create a schematic using this SS110P component and simulate, I get an error when it tries to netlist the schematic and the error is shown below.

Thanks,
Mike


Simulation / Synthesis Messages

Error detected by hpeesofsim in preprocessing during netlist parsing.
   Unable to retrieve library data: ckt:S110P (type = N)

Status / Summary


hpeesofsim (*) 2006A.400 Sep 28 2006 (built: 09/28/06 03:30:08)
Copyright Agilent Technologies, 1989-2006.
--------------------
Simulation terminated due to error.
--------------------  

Outcomes