AnsweredAssumed Answered

3GPP FDD BS TX simulation

Question asked by ccchien74 on Jan 20, 2010
I am using the ADS example file, 3GPPFDD_BS_TX_test.prj, for base station transmitter simulation.
The input source type I picked is "TestModel1_64DPCHs."
For 1 carrier signal case, it works fine.
I wonder how can I change the setup and have multiple-carrier signal in this particular source type. 

Thanks for the answer

Calvin  

Outcomes