I have downloaded a vendor library with AEL/Net/sNp etc. files. I need to load this into the Component Library list under Insert/Component in ADS layout. This will give me the footprint for each vendor device. Suggestions?
Did the vendor provide any instructions regarding how to install their library? There are several ways that librarys can be implemented for use in ADS. One of the most popular, and easy to install, is a Design Kit. If they did not provide a Design Kit, you can create a new project, place the *.ael, *.dsn, and *.net files in the /networks directory, and place the *.snp files in the /data directory. In the schematic window, you can use Tools > Custom Library to make these library parts available across a user's environment or an entire site.
Thank you for the reply. I have installed the design kit and all is well thanks to Agilent technical support. I imported the kit from the drop down menus.
Thanks for your help and reply!