AnsweredAssumed Answered

Deembedding error ADS 2006A

Question asked by s_martius on Dec 4, 2006
Latest reply on Feb 7, 2007 by wrivas
For controlling my own calculations I have used
the original Agilent deembedding demonstration project
"Fixture_deembed_prj"
With the ADS version 2006A there is an error.
The s-parameter from the deembedded DUT and DUT disagree
as you can seen here for example
f=1.0 GHz
s11_dut_deembed=0.062-j0.502
s11_dut        =0.247-j0.294
With the version 2005A the results agree.

Regards Siegfried  

Outcomes