AnsweredAssumed Answered

only one works?

Question asked by YANNING on Sep 3, 2003
Latest reply on Sep 8, 2003 by nilesh1
hello everyone,

a new problem: i have desingned in the designkit,which i have installed at user level, a few inductors mit callback function,(all of them work fine at project directory:))but a problem occured.>:( when i add a new component in the designkit, then only it works.in another word, all the others do not work any more. ???when i choose a part number from the component parameterlist,error message is the following:

(dm_get_from_definition_attribute)operand
wrong type of parameter. :-/

does anyone know the solution?  

Outcomes