Hi,
I just installed the new ADS version. No problem. But I cannot read the new license file. I get the following error message:
lmreread - Copyright (c) 1989-2005 Macrovision Europe Ltd. and/or Macrovision Corporation. All Rights Reserved. lmreread failed: Cannot read data from license server system. (-16,10009)
The license manager is version 10.8.0.1. Any idea? Please let me know.
Thank you Wolfram
I just installed the new ADS version. No problem. But I cannot read the new license file. I get the following error message:
lmreread - Copyright (c) 1989-2005 Macrovision Europe Ltd. and/or Macrovision Corporation. All Rights Reserved. lmreread failed: Cannot read data from license server system. (-16,10009)
The license manager is version 10.8.0.1. Any idea? Please let me know.
Thank you Wolfram
To support ADS 2006A, the license file should have INCREMENT lines that contain the "2.6" version. Your FLEXnet is version 10.8.0.1 which is good, since that is the version shipped with and supported ny ADS 2006A.
What about the version of your vendor daemon agileesofd and the utility lmutil? These need to be updated to 10.8.0.1 as well as lmgrd.
Recommed you:
1) Verify all your license server supporting files (lmgrd, agileesofd and lmutil) are at version 10.8.0.1 on the server. It's okay to have an lmgrd version higher than 10.8.0.1, but the agileesofd and lmutil need to be at 10.8.0.1 to support a version 2.6 license file.
2) If you are running a tri-server configuraiton (master and backup servers) it is critical that all license servers be running the identical version of the licensing files.
3) Restart the license server(s).
The lmreread is a utility embedded in the lmutil binary, and it could be that an older lmutil might not be able to communicate properly with an lmgrd/agileesofd combination of a higher version, causing lmreread to fail.
If after updating the lmgrd, agileesofd and lmutil and restarting the license server(s) you are still seeing the problem, please contact Agilent EEsof Tech Support at 800-473-3763 or eesof_support@agilent.com and we will look into the matter further.
Best regards,
Jay Mc Kee
Tech Support Engineer
Agilent EEsof EDA