AnsweredAssumed Answered

Simultanoues Simulation Instances

Question asked by eabmo on May 19, 2009
Latest reply on Jun 16, 2009 by eabmo
Hi Agilent!

I am running ADS 2009 on a PC with 4 cores.

I am looking for a way to run two simulation instances at the same time from the same project. Say for example that I am running a lengthy harmonic balance simulation and wants to run some short s-parameter simulations at the same time while waiting for the harmonic balance to finish. I have plenty of computer power so that will not be an issue. Is this possible? I understand that it is possible to start to instances of ADS but then I can not (dare not) open the same project in both instances.

Another thing that I would like to do is queue harmonic balance simulations like I do in momentum. Is that possible?

Regards
Daniel  

Outcomes